3/21/2018 5:13 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Are your sure, your application demand is master & slave? Or does it demands synchronisation? |
3/27/2018 8:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Have you studied earlier/old DC drive logic? or since two motors & drives are used so you are saying it as master & slave? In general master & slave operation is applicable where there is an additional torque requirement from load with maintaining speed constant. In you application, since two arms are operated independently, its motion needs to be synchronise. However as deriered by you please refer Parallel or series connection of motors to understand DC motors connection in parallel or in series. HTH. |
3/30/2018 5:27 PM | |
Posts: 69 Rating: (4) |
How to apply electromagnetic braking in motor? |
Follow us on