11/6/2007 4:38 AM | |
Joined: 5/19/2006 Last visit: 4/17/2024 Posts: 548 Rating: (107)
|
Hi, In this case did you try to enable "Display error dialog" under Computer properties -> Runtime VBS-Graphics and see if you get the Pop-up dialog? (see attached) The prerequisite for this function is that a Debugger for Visual Basic must have been installed. Dec Attachmentmessage.zip (119 Downloads) |
Last edited by: Dec at: 06.11.2007 04:44This is strange: I typed D_e_b_u_g_g_e_r and it shows De*** Last edited by: Dec at: 06.11.2007 04:42This is strange: I typed <Debugger for Visual Basic> and it shows De*** Last edited by: Dec at: 06.11.2007 04:39 |
|
11/6/2007 4:03 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
Hello ilya_v and Dec, D_e_b_u_g_g_e_r is shown as De*** you are right. Here the reason: Have you ever tried to read the word without the "De"? So it is a censored word within our Technical Forum. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
8/15/2008 12:00 PM | |
Joined: 12/13/2005 Last visit: 3/29/2024 Posts: 61 Rating: (3) |
Hello Ilya_v, Have you already found the solution for this problem. I'm stuck with exactly the same. greetz, Bart. |
8/15/2008 1:53 PM | |
Joined: 12/13/2005 Last visit: 3/29/2024 Posts: 61 Rating: (3) |
Hello to all, This was the reason of my problem: On the BAD PC ther was no OFFICE installed. And for some reason what so ever there was also no debugger installed by WinCC. So I downloaded on the microsoft site te "Microsoft script debugger" and installed it on the server. Now everything works like it has to Below is the link to the site from microsoft: http://www.microsoft.com/downloads/details.aspx?familyid=2F465BE0-94FD-4569-B3C4-DFFDF19CCD99&displaylang=en succes to all with the same problem greetings, Bart. |
Follow us on