11/21/2014 11:46 AM | |
Posts: 19 Rating: (0) |
Hi All, Wincc V7.0 SP3 software is installed in Windows 7 ultimate 64 bit OS. Configured a TCP/IP connection for establishing communication with S7317 PLC through CP343-1lean module. IP used : 192.168.0.90 in PLC & 192.168.0.100 in WINCC S7 Connection details : IP 192.168.0.90 Slot 0 Rack 2 System parameter : selected as realtek Ethernet port of WINCC PC. even put all setting properly, communication is not establishing between wincc & CP343-1lean please Note: I have established a communication using windows XP OS with same settings in wincc. In Windows 7 OS, i got exclamatary mark on netwrok connection & "undefined network" is showin of taskbar. I dont know what is wrong with this project or system.Please suggest anybuddy who have faced similar problem. Thanks in advance, Prabhu Kumar V AttachmentDesktop.zip (72 Downloads) |
Last edited by: Min_Moderator at: 11/21/2014 1:27 PMRenamed attachment |
|
11/21/2014 2:35 PM | |
Joined: 5/19/2014 Last visit: 3/5/2024 Posts: 29 Rating: (1) |
Hi: Are you sure you select the right ethernet adapter in wincc, tcp/ip driver properties? Regards Darío Fernández |
Follow us on