3/26/2018 12:32 PM | |
Joined: 8/3/2009 Last visit: 4/19/2024 Posts: 12816 Rating: (1634) |
Hello Mr.ananda I would say if the standby Station is configured exactly as the one you use for Server then It should work if you do an exchange of the Hardware. Of course you should try almost once a year also to check if your Cold Standby Hardware still works. Here Information to the CP1613 https://support.industry.siemens.com/cs/ww/en/view/2361347 |
If this Information really helps, you could use the Rate function |
|
3/29/2018 7:53 PM | |
Joined: 11/1/2016 Last visit: 1/23/2024 Posts: 17 Rating: (0) |
Sir, After new CP 1613 card and all supporting software installation in a new server. Can it possible to work the existing project without any changes NetPro. I want to change server one to one replacement. Can it possible ?
|
Last edited by: Mr.ananda at: 3/29/2018 8:01:26 PM |
|
Follow us on