4/27/2018 12:30 PM | |
Joined: 11/15/2010 Last visit: 1/8/2024 Posts: 13 Rating: (1) |
Hi Sorry i don't checked if the file was present becase i have uninstalled the program. I attached the new one, for this installation. This time i see the same error for "starter V5.1.1.2" installation, and the final errors during the configuration files, but i havent error during the configuration of simatic ET200pro. But the program still not work, and closing with "the application has encountered a problem and needs to close" when i open it (double click on desktop icon). If can be helpful, the folder "ssp_simotion_int_v4.4" is created in the last part of installation, like last but three part. Thanks again Attachmentmkcfgdbdr.bat_Log.txt (506 Downloads) |
4/27/2018 12:41 PM | |
Joined: 11/15/2010 Last visit: 1/8/2024 Posts: 13 Rating: (1) |
Hi Yes, i have this one Thanks AttachmentInstall_SSP_SINAMICS_SIMATIC_ET_200PRO_FC_2_V4_7_9__04.79.10.02_Log.txt (547 Downloads) |
4/27/2018 12:45 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
is also available the file hwkatimport_SSP_SINAMICS_SIMATIC_ET_200PRO_FC_2_V4_7_9__04.79.10.02_Log.txt? |
4/27/2018 1:55 PM | |
Joined: 11/15/2010 Last visit: 1/8/2024 Posts: 13 Rating: (1) |
Yes over there Thanks Attachmenthwkatimport_SSP_SINAMICS_SIMATIC_ET_200PRO_FC_2_V4_7_9__04.79.10.02_Log.txt (471 Downloads) |
5/2/2018 9:05 AM | |
Joined: 11/15/2010 Last visit: 1/8/2024 Posts: 13 Rating: (1) |
Hi Any news please? |
5/3/2018 5:38 PM | |
Joined: 11/15/2010 Last visit: 1/8/2024 Posts: 13 Rating: (1) |
SOLVED!! I think the problem was the old installation of starter, v4.3 and v4.5. I had uninstalled them but ramaining some old files stored in PC folders. So i had uninstalled Starter and other parts of the program, like Microsoft office acces database engine, Microsoft visual C++ redistributable 2008, Simatic Step7 v5.6 +HF1 OEM2. Reboot Clean registry key and Windows temp folder with a program like CCleaner, and deleted some folder of the program, that still remaning on the pc after the uninstall process: \\program data\Siemens\automation\ simatic oam, step7, sws, trace engine. And also here \\program (x86)\Siemens\ step7. and rebooted again. Now, with Windows UAC disabled, antivirus disabled, sreen saver disabled and step 7 microwin allready uninstalled; I launch setup.exe again, and this time Starter installed correctly I posted the solution here, hope this will be useful for someone other. Thanks anyway for the help, bye |
This contribution was helpful to3 thankful Users |
Follow us on