5/3/2018 9:27 AM | |
Posts: 5 Rating: (0) |
Hello, I would like to assign PROFIsafe adress of the differents modules but there is one that I can't assign (picture 001) (F-DI8x24 VDC HF with the article number 6ES7 136-6BA00-0CA0). There is "aborted" on his status (picture 002). When I look on diagnostic status I have 2 errors : 16# 0D:75E5 Safety program : F-I/O passivated 16# 0D:75D3 Safety program : Error in PROFIsafe communication with F-I/O I check my DI parameters (pictures 003 and 004). The LED "Diag" on the module is flashing in red and the LED "PWR" is in green in continuous. The next module is working. Have you an idea, please ? Thanks by advance. Attachmentpictures_errors.zip (1057 Downloads) |
This contribution was helpful to1 thankful Users |
7/20/2022 4:50 PM | |
Joined: 8/28/2017 Last visit: 7/5/2024 Posts: 30 Rating: (1) |
For me restart of CPU worked |
This contribution was helpful to1 thankful Users |
Follow us on