4/26/2018 1:52 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi kopo_vagyok, I hope your ES station is a Siemens IPC847D or some sort. If so, you can use the supplied restore disks to have your system set back to a clean Windows 7 before install of PCS7 V8.2. Then you can install PCS7 V8.2 after the restore is complete. However, if you are using a desktop/laptop non Siemens, then the only good way is to reinstall Windows and then PCS7. You can uninstall all Siemens software, but it is tricky and in the end, reinstall of Windows + PCS7 is a bit more time consuming, but the good way. If you a smart, you reinstall Windows and make an image before installing PCS7. Maybe you can also check your computer for a restore point (if activated). If so, maybe you have an option to use a restore point before installing PCS7. |
If I could help you, you can use the RATE button. Thank you. |
|
4/26/2018 6:24 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
"Without the re-installation of the computer please" This is not recommended. If you do this and make some tests, the results/behaviour might be different to the behaviour of a normal (new installed) system.
|
Last edited by: Thunderstorm at: 4/26/2018 6:25:13 PMSIMATIC PCS 7 - Overview |
|
5/8/2018 7:15 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi kopo_vagyok, Did you find a solution, or what did you decide to do? I'm curious |
If I could help you, you can use the RATE button. Thank you. |
|
5/8/2018 8:23 AM | |
Joined: 1/13/2016 Last visit: 8/29/2022 Posts: 37 Rating: (0) |
Hi, as you recommended, the windows reinstall :) |
5/8/2018 8:56 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
the only good way.. Re-installing may appear faster, but the chance of getting problems is substantially. You don't want that in a running factory.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on