1/11/2017 9:25 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi, In order to use AddFEM blocks, you will need the driver blocks. You can install these from the supplied CD. See the attached print screen. The screenshot is taken from the Getting Started manual. You can find the manuals HERE Search all AddFEM manuals by opening: Add-ons for SIMATIC PCS 7->Distributed I/O on the PROFIBUS and there you find the following manuals: AddFEM Sequence of Event AddFEM Getting Started AddFEM Front End Module ADDFEM PCS7 Driverblocks The manual Getting Started describes the exact procedure on how to use AddFEM. Edit: I see the latest edition is from 2006.
|
Last edited by: Oreca at: 1/11/2017 9:31:04 AMLast edited by: Oreca at: 1/11/2017 11:26:51 AMIf I could help you, you can use the RATE button. Thank you. |
|
1/11/2017 9:37 AM | |
Posts: 111 Rating: (15) |
Hello, it is difficult to find some information about this issue. There is no information about a compatibility between PCS V8.2 and Add7 AddFEM (last information is PCS7 V6.1) Did you see the following information, which may help you: The driver block: https://support.industry.siemens.com/cs/ww/en/view/79724754 Getting started: https://support.industry.siemens.com/cs/ww/en/view/79723556 If you won't get more information, you may open a support request: https://support.industry.siemens.com/My/ww/en/requests Hopefully this might help you a little bit.
|
5/5/2018 8:56 AM | |
Joined: 5/14/2015 Last visit: 9/26/2023 Posts: 1 Rating: (0) |
Hi Have you got some solution? Because I Have got the same problem.. Thanks R. |
5/9/2018 9:08 AM | |
Joined: 6/19/2008 Last visit: 8/6/2024 Posts: 46 Rating: (4) |
Hi, For PCS7 8.2 you need dedicated AddFEM Library 8.2 AttachmentReadme.pdf (122 Downloads) |
Last edited by: Kargan at: 5/9/2018 9:08:37 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on