4/28/2016 6:03 AM | |
Joined: 4/28/2015 Last visit: 12/21/2021 Posts: 9 Rating: (0) |
Dear Experts, Recently I have found a problem in client station. Suddenly the Runtime stopped and shows grey screen with the text: "This station has an inoperable status Please inform your service management or restart the computer" The only thing to do is to click a red button in the bottom right corner to restart the PC. The only explanation I got is from the manual Process Control System PCS 7 OS Process Control (V8.1) with document number A5E32785344-AA on section 5.4.9. And this doesn't give a lot of information. Has anyone experienced this kind of problem? My Multiproject is based on PCS 7 V8.1 + SP1 and CEMAT V8.1 Regards, Fred AttachmentCLIENT_ERROR.zip (730 Downloads) |
Follow us on