4/26/2018 8:59 AM | |
Joined: 1/8/2011 Last visit: 5/29/2024 Posts: 4 Rating: (0) |
Dear members, I added some packages like openvpn in the "iot2000-example-image.bbappend" file. This works fine, the image is booting and i can connect to the iot using the example image ip .200.1.
What is wrong with my own recipe? Kind regards! Attachmentqmithings_1.0.txt (154 Downloads) |
Last edited by: SeebaN at: 4/26/2018 9:02:04 AMcouldnt post the file content as code within post |
|
4/30/2018 10:16 AM | |
Joined: 1/8/2011 Last visit: 5/29/2024 Posts: 4 Rating: (0) |
Has no one any idea what is wrong with the recipe? |
5/2/2018 2:57 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60) |
Hello Sebastian, You may be right about something going wrong in init.d. I'm also a bit unsure about line 29 in your recipe:
You could try to add this initscript differently, like in this example: Need help with an initscript bitbake recipe Kind regards! |
This contribution was helpful to1 thankful Users |
5/14/2018 5:36 PM | |
Joined: 1/8/2011 Last visit: 5/29/2024 Posts: 4 Rating: (0) |
Hello Felipe, this solved my problem. Many thanks to you! |
Follow us on