5/11/2018 2:05 PM | |
Posts: 21 Rating: (0) |
Dear Team, i am facing a problem Analog Card (6ES7 331-7KB02-0AB0) was not detect by CPU312 (6ES7 312-1AD10-0AB0) and CPU in STOP mode even OB80, OB82 was in program and after cold and warm start CPU not going to RUN mode. List of activity is below which is followed but still problem is same :- 1. Check 24VDC 2. Complete Power OFF and ON for system 3. Changed analog card with 2 new card with same type no 4. Changed back bus connector with new one 5. Remove all field wiring only 24VDC is connected 6. Complete program download including hardware configuration For Reference following Screen shots attached :- 1. Hardware Configuration 2. Analog parameter Settings 3. Diagnostic Buffer Please Suggest......... Thanks & Regards....... AttachmentScreen Shot.zip (79 Downloads) |
5/14/2018 8:55 AM | |
Posts: 21 Rating: (0) |
Dear Sir, Please find the Diagnostic buffer details. Please suggest. AttachmentDiagnose.txt (68 Downloads) |
5/14/2018 9:08 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi, is this a new configuration or was it already running? regards, |
FCK WAR! |
|
5/14/2018 2:30 PM | |
Posts: 21 Rating: (0) |
Hi, Its a same configuration just change the real time clock . Problem still same Today i am try with changing the position of the card with digital output card in hardware configuration as well physical hardware but Problem is same with analog card with same error. PLC backup is attached for reference . Error Details is :- Event 1 of 100: Event ID 16# 49A2 Please Help Me !!!!!!!!!!!!!!!!!!!!!!!!!! Thanks ......... Ashish Vijay AttachmentPLC Backup.zip (61 Downloads) |
5/14/2018 3:47 PM | |
Joined: 10/16/2007 Last visit: 2/23/2024 Posts: 627 Rating: (45) |
Did you change the CPU? I sometimes had different strange faults when the CPU was broken. Regards |
5/15/2018 9:16 AM | |
Posts: 21 Rating: (0) |
Hi,
|
Follow us on