5/15/2014 12:31 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Jumo, I will check this out, maybe in there is a solution Thx for the feedback! |
If I could help you, you can use the RATE button. Thank you. |
|
8/4/2014 11:38 AM | |
Posts: 62 Rating: (2) |
Hi, I have the same problem. We found out that after not set 'master library', CFC editor seems to work faster. Hope this may help. :) |
9/24/2014 2:00 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Yuwanee, It indeed works with me when removing the master library. Today I installed PCS7 8.0 SP2 and the opening of charts is fast as it should be WITH a master library. Problem seems to be solved in SP2. What it was I dunno, but I love it |
If I could help you, you can use the RATE button. Thank you. |
|
9/24/2014 3:37 PM | |
Posts: 5 Rating: (0) |
Yes, after instalation SP2, it works like charm. Hopefully will not be the same problem in PCS7 version 8.1, which will be released soon. |
5/24/2018 12:30 PM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 8002 Rating: (163) |
New question published by mujahid143 is split to a separate thread with the subject where is the exact location of these .alarm logs?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on