6/6/2018 7:33 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello syd_b, you can not change the cycle-time for a archive-tag, you have configured in the Taglogging during runtime by an user. If you would like to archive a value only once a day, and the user should trigger the event for this, you could use for "Acquisition type" the option "acyclic" and use an internal Tag (Bit) for the "Start tag" and "Stoo tag" which the user sets/resets by mouseclick. Or you use the ODK-function "TLGInsertArchivData" in an C-script, to insert data directly in the Taglogging-Archive. Best Regards Georg Berghof AttachmentTLGInsertArchivData.pdf (123 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on