6/12/2018 5:40 PM | |
Posts: 6 Rating: (0) |
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/13/2018 9:11:23 AMNew subject after splitting |
|
6/13/2018 9:38 AM | |
Joined: 7/9/2015 Last visit: 5/8/2024 Posts: 3820 Rating: (555)
|
Hi dinsss, for PLCSIM you need for each PLC an own PLCSIM instance - please check the following example, where a connection between two PLC with PLCSim is described: How do you simulate a communication between two S7-400 CPU modules with STEP 7Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
6/13/2018 9:42 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, Are you usingPLC-Sim? If yes, then you need two PLC-Sim instances for this. There is also a FAQ where two PLCs are communicating in PLCSim: How do you simulate S7 Communication between two S7-1500 CPUs using S7-PLCSIM V13?hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on