7/24/2012 2:42 AM | |
Posts: 8 Rating: (0) |
Has anybody looked at or even used www.myscada.org yet? It looks like a great way to talk to a network of logos, especially if it can talk to S7 devices. I really want to know if anybody has used it to talk to a logo. Mem |
This contribution was helpful to1 thankful Users |
7/24/2012 5:33 PM | |
Posts: 378 Rating: (73) |
Hello, I have seen the software before it is a graphics editor, All I can understand is it is ony for s7-300/400/1200 by using myScada Box hardware for the router. Not for the LOGO! Here is how it works S7-PLC>>> myScada Box >>> SCADA server with SQL database >>> myScada Box>>> iPad/iPod/iPhone I can't see any advantage to use it! If its only for S7 families, I know I can do like this: S7-PLC>>>SCADA server with SQL database>>> iPad/iPod/iPhone/Android>>>S7-PLC OR S7-PLC with bluetooth/wifi <<<>>>Android Once again NOT for the LOGO! Regards, |
This contribution was helpful to2 thankful Users |
Follow us on