6/18/2018 10:08 AM | |
Joined: 11/7/2016 Last visit: 4/20/2024 Posts: 16 Rating: (2) |
hi, here I attached sql setup log and summary file, please go through it. Overall summary is : Final result: Failed: see details below Exit code (Decimal): -2068709375 Exit facility code: 1202 Exit error code: 1 Exit message: The patch file cannot be opened.
Attachmentwincc-sql-error-log.zip (290 Downloads) |
6/18/2018 11:15 AM | |
Joined: 11/7/2016 Last visit: 4/20/2024 Posts: 16 Rating: (2) |
Hello Christoph, Thanks for suggestion. But still error not solved even after folder name modified. here I attached summary. Overall summary: Final result: Failed: see details below Exit code (Decimal): -2068709375 Exit facility code: 1202 Exit error code: 1 Exit message: The patch file cannot be opened. The file is: D:\SOFT\NEW_3\InstData\SQL\SQL2014STDSP1\setup\PCUSOURCE\1033_ENU_LP\x86\setup\sql_dqc_loc.msp. Is there another solution ? Thanks in advance. Regards, Pravin AttachmentSummary.txt (183 Downloads) |
Follow us on