6/30/2018 11:07 PM | |
Joined: 1/30/2018 Last visit: 7/16/2024 Posts: 14 Rating: (0) |
I translate the text, it takes a moment |
6/30/2018 11:21 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
You can take your time, for me today is over. |
6/30/2018 11:30 PM | |
Joined: 1/30/2018 Last visit: 7/16/2024 Posts: 14 Rating: (0) |
OK thank you |
7/1/2018 3:53 PM | |
Joined: 1/30/2018 Last visit: 7/16/2024 Posts: 14 Rating: (0) |
Hallo ixo65, I tried to translate the project. activation of language change over M29 Perhaps it is understandable. My problem is in the B127 Rain Sensitivity setting screen. The password in the setting is the number 1. On the setup screen, I want to change the set point value via the cursor key. It changes to the UP / DOWN counter B129 but does not jump into the B119 analog treshold triger. In the simulator, this value is precious but in real Logo8 it is not.I need the CNT value from B129 to automatically transfer to ON in B119 Thank you Attachmentsvetliky.zip (137 Downloads) |
7/1/2018 5:05 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
The transfer of the value from "B129 Ax" to "B119 ON" works perfectly. If the input value of B119 is greater than the ON value, the threshold switch turns on. If the input value of B119 is less than the OFF value, the threshold switch turns off. I checked this online in a real LOGO! 8.2. The value transmitted by B129 will not be displayed to you online on B119 because it is referenced. The value of B119 at the output will be displayed on B119. AttachmentB119 Online.zip (159 Downloads) |
Follow us on