7/12/2018 11:05 AM | |
Posts: 3 Rating: (0) |
Hello All! I'm trying to create first SIMATIC IOT2000 project using SIMATIC_IOT2000_Getting_Started_V2.0.2%20.pdf. Has can be seen on the attached image, two include directories are not resolved because they refer to directory C:\Users\Matt\Documents\IOT2040\V2.2.0_SDK_Windows\sysroots\i586-nlp-32-poky-linux\usr\include\c++\5.3.0 , but in effect in the directory C:\Users\Matt\Documents\IOT2040\V2.2.0_SDK_Windows\sysroots\i586-nlp-32-poky-linux\usr\include\c++there is \6.2.0 instead of \5.3.0 Very probably this is due to the fact that i Installed SDK version 2.2.0 Instead of 2.1.2? If Yes where can I download the older version? Or how can otherwise be solved this problem? Thank You ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/12/2018 12:18:46 PMNew subject after splitting |
|
7/12/2018 12:51 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, please see this entry in the forum. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on