1/17/2018 12:18 AM | |
Joined: 10/26/2013 Last visit: 9/20/2024 Posts: 47 Rating: (5) |
Try upload. :-) |
This contribution was helpful to1 thankful Users |
7/25/2018 7:32 AM | |
Joined: 4/30/2018 Last visit: 9/27/2022 Posts: 1 Rating: (0) |
From Help Download Click this command to download a LOGO! Web Editor project from PC to the Micro SD card of LOGO! Base Module. You can also use this button in thestandard toolbarfor such purpose. Upload Click this command to upload a LOGO! Web Editor project from the Micro SD card of LOGO! Base Module to PC. You can also use this button in thestandard toolbarfor such purpose. |
Follow us on