8/7/2018 8:31 AM | |
Posts: 20 Rating: (0) |
Is possible to connect to logo 8 by web with multi session? I see that using the same user, the last login close the precedent one and just one session can exist. Is possible create more users or use a workaround? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: pgbuz at: 8/7/2018 8:31:22 AMLast edited by: Jen_Moderator at: 8/7/2018 10:25:48 AMNew subject after splitting |
|
8/7/2018 9:00 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Have it still tested with the web server: Registered with 2 devices at the simple web server, first with the tablet and then with the PC: Registered with 2 devices at the extended web server, first with the tablet and then with the PC: AttachmentErweiteter Web Server Mehrfachzugriff.zip (34 Downloads) |
Follow us on