5/11/2012 7:24 AM | |
Posts: 26 Rating: (0) |
Hi All, thanks for Your replies. I'm glad that I can use the hardware I already have:) Ammy I read about it on PPI MPI protocool manual, but in Polish language. However if Your interested, there are pictures with PPI (page 3), and MPI(page 5). It's written there, that to connect with S7-200 You need a PC station with rs232/485 converter. Then on the picture there is PC/PPI converter(RS232/RS485) Thanks a lot With best regards Karol AttachmentInterfejsy_PPI_MPI_.PDF (927 Downloads) |
5/11/2012 7:29 AM | |
Posts: 1064 Rating: (72) |
yes fo ra pc that is true you need a converter but not for a field pg as Ammy stated the cp card built into the pg has the converter built in |
2/8/2014 5:11 PM | |
Posts: 340 Rating: (6) |
new question is splittet to MPI cable to connect to s7-300 PLC, ICP RS-232 to RS-485 Converter |
Follow us on