1/14/2016 11:08 AM | |
Posts: 75 Rating: (1) |
Hi friends, I didnt understand this, is it possible to do it without buy a Static IP ? because it is expensive in my country.. |
6/21/2016 7:51 AM | |
Posts: 3 Rating: (0) |
Dear Gaspar1, I will try to connect to a s7 1200 PLC remotely by following your step but i have a few questions. If you don't ming, can you help me, please? For examplei i am far away from PLC and i want to connect it. I have to make these steps on the PLC site to connect ??? The router is from PLC site ?? Not mine? I confused a little... Thanks for all Best Regards ARS16 Step 1.Create a web server application and download it to S71200 Step 2.Testing web server application in LAN
Example: IP address of my PLC is 192.168.0.12 (Subnet mask 255.255.255.0., Router 192.168.0.1) I type in URL tab:http://192.168.0.12
Step 3.By Static IP address from your Internet provider,
Step 4.Router settings
(My router settings in attachments) Step 5.Remote testing
(80 - port number) Step 6. ENJOY!!!... Dragan MarinkovicGreetings from Belgrade, Serbia |
7/16/2016 11:42 PM | |
Posts: 146 Rating: (7) |
Thanks on explanation, only after forwarding port 443 my web server started to work over static IP address. Svaka čast na objašnjenju, spasio si me danas! :-) Pozdrav, Miloš |
Follow us on