8/30/2018 4:03 PM | |
Joined: 2/26/2009 Last visit: 7/21/2020 Posts: 6 Rating: (0) |
I have an Italian assembly machine that uses CAN bus for I/O which then goes thru an ESD CAN to DP bridge to the S7-315 2DP. I am bringing this machine back to life after 2 years in storage but the CPU battery had failed. I have had great assistance from folks at ESD and the machine is running now but we continue to have random momentarily CAN bus data freezes. I am able to capture the CAN data in a trace file and don't see any reports of frame errors or other errors. I do see RTR requests at address 070A which never get a reply. Could this be a problem? If I have electrical noise on the CAN bus how would that show up in the trace data? Any help would be appreciated. Doug AttachmentT052 trace 0822 1713.txt (97 Downloads) |
Follow us on