8/19/2018 8:05 AM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Dear All, Presently I'm working in Softstarter 3RW4423-3BC44. In this Softstarter 02 inputs & one output has been used to control a motor in Dual direction. The dual Direction of motor is controlled in Hardware mode. In manual mode of operation from PLC logic the softstarter is operating in normal mode & the motor is rotating in both directions. Now when I've developed the Auto operation control, in forward direction the softstarter is behaving normally but when the sequence comes to change in direction reversal, the softstarter is getting tripped & fault on display is showing "No Power". One input is set on Motor Right with PS1 & other is set to Trip Reset Parameters. Do I've to set another input to Motor Left with PS1 or to Quick Step parameter? I've attached the Backup of both PLC & Softstarter, kindly help me for solving this problem! Regards OmKris AttachmentStacker.zip (175 Downloads) |
9/2/2018 9:06 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
ZIP folder did not open. Could you please attach PLC & Softstarter back up independently/separately? |
Follow us on