11/29/2017 2:59 PM | |
Joined: 7/9/2015 Last visit: 4/24/2024 Posts: 3812 Rating: (554) |
Hi, please also check PDF Page 120 - table 22.2.5 S7-1500 to PB CPU-CPU Communication with SIMATIC ControllersRegards, Towome |
|
|
This contribution was helpful to1 thankful Users |
11/30/2017 3:02 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello; If I understood your first task correctly you have a S7-1542-5 as a DP-master connecting to a DP/DP coupler setup by a third-party programmer with a S7-300 DP-master. What do you know of the function of a DP/DP coupler? you should know it is a special DP-slave with 2 interfaces; one interface must be connected and configured to the S7-300 DP-master (in your project), the other must be connected and configured to the S7-1500 DP master. Next the data exchange areas must be setup properly: the trick is that output addresses on the S7-300 side must correspond to input addresses on the S7-1500 side, while the input addresses of the S7-1500 side must correspond to the output addresses of the S7-300. That allows data written to the S7-300 coupler side to be read by the S7-1500 side, and vice-versa. DP/DP Coupler, how to configure it? So, basically, the main question is: did you get information from the 3rd-party programmer about the data exchange structure he has implemented on the S7-300 side of the DP/DP coupler? If not, fdo you have access to his Hardware configuration to find that out? Your second task consists of setting up the S7-1242-5 as a DP-slave to a S7-300 DP-master. Here are a few discussions from the forum that will help you understand the steps to do so: Integrating CM 1542-5 as I slave in STEP 7 V5.x - Industry Support Communication of S7 1500 & S7 400 over Profibus - Again, the main question is: do you know the data exchange structure that needs to be implemented between master and slave?. This is critical to the success of your project. Also, you have to be able to integrate the S7-1500 slave to the S7-300 master begfore the DP link is functional. Do you have access to the S7-300 PLC program, or can you hacve help from the 3rd-party programmer for this? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/30/2017 3:08:18 PMLast edited by: Jen_Moderator at: 11/30/2017 3:09:01 PMInserted right links. |
|
This contribution was helpful to1 thankful Users |
Follow us on