9/12/2018 11:41 PM | |
Posts: 10 Rating: (0) |
Hello everyone, Attached is a list of active processes on my Siemens device (ps -A > active_process.txt). There are several applications (daemons) running in the background. Is there a way to: 1. Determine which of these are critical for system operation and which are not? For example, ipv6_addrconf (PID # 73) isn't required for my applications since I need only IPV4. 2. Remove modules & applications without having to rebuild the entire image from scratch? So in the example above, I would remove IPV6 from /etc/modules. But I am looking for a more generalized approach. I apologize if the question is too broad or vague but any suggestions or feedback would help! Thank you! Nester Pereira Attachmentactive_process.txt (248 Downloads) |
Follow us on