9/14/2018 11:04 AM | |
Posts: 1 Rating: (0) |
Dear sir, With the maximum 12A inrush current at 28.8V Can we apply the power suppy 24V, 5A for PLC S71200 DC DC DC ?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/14/2018 11:42:38 AMNew subject after splitting |
|
9/14/2018 11:24 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Yes, no problem Single-phase, 24 V DC (for S7-1200) - Industry Mall - Siemens WW |
9/14/2018 12:12 PM | |
Posts: 2826 Rating: (685) |
Hello.
I have never noticed that specification before. 12A@28.8V inrush.. wow!
Regards. |
Last edited by: #dP at: 9/14/2018 12:12:45 PM |
|
9/14/2018 12:21 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello #dP, in fact, I posted to him this PSU that for a CPU 1200 is enough even with 2.5A |
This contribution was helpful to1 thankful Users |
Follow us on