9/11/2018 12:39 PM | |
Posts: 11 Rating: (1) |
Dear All I have a CPU 313C-2DP (6ES7313-6CG04-0AB0) and I want to use DPV1 Master functionality. I've seen in CPU datasheet that DPV1 is supported as DP Master for this type of CPU. But in the property dialog of CPU313C-2DP (DP-Operating Mode tab) there is no option for selecting DPV1, while for S7-400 CPUs it can be selected between DPV1 and S7-compatible (Attachment) Please give me your advise, how should I enable DPV1 for S7313C DP master? Sincerely AttachmentDPV1.pdf (97 Downloads) |
9/11/2018 12:49 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, please have a look below: How can you tell whether your S7-300/400 master supports DPV1 ... Product Information Conversion to DPV1 FAQ ... - Siemens Support Attachmentleitfaden_e_0103.pd.pdf (92 Downloads) |
Last edited by: Jen_Moderator at: 9/11/2018 2:49:03 PMOptimized link and added file as an attachment. |
|
This contribution was helpful to1 thankful Users |
9/11/2018 2:40 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello NaAhoora; An even more fundamental way of determining if your CPU supports DPV1 services as a DP master: check the Technical data of the cPU: https://support.industry.siemens.com/cs/pd/308335?pdti=td&dl=en&lc=en-WW To find that link, write the part number of the module you are looking for in the Search box at the top right of this page, click to search, open the Product links link in the results page and open the Technical data tab. There you will find the contents seen in the screenshot below. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
9/26/2018 9:56 PM | |
Posts: 11 Rating: (1) |
Dear Friends Thank you so much for your suggestions. I considered the following: How can you tell whether your S7-300/400 master supports DPV1 ... Product Information Conversion to DPV1 FAQ ... - Siemens Support It made me more confused! The first link proposed a procedure to detect which s7300 CPUs supports DPV1. I've installed the GSD V5 for IM153-2 (6ES7 153-2BA01-0XB0), unlike what is said in this procedure, after installation of GSD, still it's not possible to change between DPV0 and DPV1 in DP operating mode off CPU. The secondlink, stated "In the S7-300 family, the CPUs with MMC support the DPV1 master functionality as of firmware version 2.0" So what?! I have a simple and clear configuration: a CPU313C-2DP is connected to IM153-2 (6ES7 153-2BA01-0XB0) via onboard DP port of CPU, like attachment (DPV1.pdf). Is it possible to use DPV1 functionality in such a configuration?! Sincerely AttachmentDPV1.pdf (94 Downloads) |
Last edited by: NaAhoora at: 9/26/2018 9:56:50 PM |
|
Follow us on