9/14/2018 7:30 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello Ahmed; Just for clarification on your part: which version of WinCC are we talking about? WinCC v7.x, WinCC Professional or Advanced Runtime (TIA Portal), WinCC Flexible Runtime? This is an interesting page from ABB's support forum; you should find enough hints to help you out: https://forum-controlsystems.abb.com/10317/AC800M-WinCC-HMI They suggest 3 connections: OPC, Profibus (Using CI854A), and Modbus TCP. The original poster states (wrongly, in my opinion, that WinCC supports Profibus only with Siemens PLCs, and Modbus TCP only with Modicon PLCs I have connected WinCC v7.x with various PLCs from different manufacturers in the past. But of course you will have to create your tags by hand in WinCC. So basically they recommend OPC as a main connexion. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
9/14/2018 8:05 PM | |
Joined: 11/15/2015 Last visit: 4/21/2024 Posts: 178 Rating: (28) |
Dear dchartier, Thanks a lot for your replying, i read that. I want to migrate it to WINCC 7.x, also my suggestion that i will keep the ABB 800XA SCADA as it it's to avoid any problems, And i want to create the new project by WINCC in another PC with profibus communication, My question how to make my project communicate parallel with the old one ABB 800XA? Another thing to create tags manually for all plant is big task it will tak more time? Is there any way to export to .csv file or anything. Many thanks |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
9/27/2018 5:08 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, in this case I would recommend to create a service request: https://support.industry.siemens.com/cs/ww/en/sc/2090 Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on