9/23/2018 6:45 PM | |
Posts: 5 Rating: (0) |
In the design interface, the pipes are linked, but when the simulation starts, the interface is faulty, the pipes is removed. How can fix this error? tran duong
|
9/24/2018 6:29 AM | |
Posts: 5 Rating: (0) |
No, I have not yet written the code, the error here is when running the wincc simulation, the image is not as designed. (As in the picture) |
9/27/2018 5:35 AM | |
Posts: 5 Rating: (0) |
I don't use any animation, I don't understand why the objects when running simulations incorrectly positioned as designed. |
9/27/2018 3:17 PM | |
Joined: 4/20/2016 Last visit: 3/25/2024 Posts: 23 Rating: (3) |
hello, Regards |
9/27/2018 6:40 PM | |
Posts: 5 Rating: (0) |
Hi, all. I chose 1600x900 resolution for both "Options => settings" and "properties of screen". And what do you mean "the real runtime system?", Mr. Prof. Frink. |
9/28/2018 3:47 PM | |
Posts: 5 Rating: (0) |
Hi, Hati. Where is the resolution setting of the PC Runtime and the PC Engineering Station? Can you guide me? Thank you very much!
|
Follow us on