3/31/2010 3:46 PM | |
Posts: 99 Rating: (7) |
Do you have a multie project? How is time-of-day synchronization configuredby Industrial Ethernet in PCS 7? -for WinCC is it the same Synchronizing the time for PCS 7 V5.x via CP1613 => for WinCC is it the same
|
10/2/2018 9:00 AM | |
Posts: 1 Rating: (0) |
In order to synchronize the redundant pair you need to separately synchronize them to a master via WinCC system bus or through NTP as a NTP Client. |
Follow us on