10/7/2018 2:09 PM | |
Posts: 10 Rating: (0) |
Hi! I am running Tia porta V14 update 6 and this doesn't work. I changed the path to the temp folder and it creates the file but what happens when reading with lineinputstring is that it reaches the end of the file in the 4th line, can anyone help me with that? Many thanks, Raúl
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 08.10.2018 10:26:23Neue Überschrift nach Splitten |
|
10/8/2018 9:42 AM | |
Posts: 10 Rating: (0) |
Hello Prof.Frink, Now is working, but is something weird. This is the code I was running, I used some indexers so I could see where was it getting stuck. I attach the two txt that two different screens were generating. The one that has DNS on it ends at the 4th row and the other one at 31st. I deleted the DNS and guess what? Is also working. Does anyone know why?
AttachmentIP.txt (165 Downloads) |
10/8/2018 9:43 AM | |
Posts: 10 Rating: (0) |
And the other txt
Attachmentip_12.txt (181 Downloads) |
Follow us on