10/9/2018 6:34 PM | |
Posts: 50 Rating: (0) |
Its me again! The directors have finally parted with the funds to start the system. I have purchased the CPU, HMI and network switches and created the network. Now i just need a small hand on how to create the analog input scaling, as you can see from the attached images i have made an attempt but i would appreciate some help on how to configure the KTY84 thermistor into a analog input. Also the network switches Scalance XB004-1 have SC fibre connectors? the IT department and given me a small SC om4 cable to work with. Thanks again, Matty Green AttachmentDoc1.docx (133 Downloads) |
10/11/2018 8:44 AM | |
Posts: 50 Rating: (0) |
Good Morning, I have attached some print screens of the new configuration. From the datasheet it says that the resister has a value of 970-1030, am i correct it applying 3kohm in the measurement settings? Also am i correct in scaling the temperature to the min and max stated on the datasheet? Is there a way of having of monitor displaying the image of the HMI (49inch tv)? I will be monitoring 4 machines at the same time so i would like my HMI to switch between machines every 15 seconds, is this possible? Thanks for your help in advance, Matty Green AttachmentDoc2.docx (129 Downloads) |
10/18/2018 2:17 PM | |
Posts: 50 Rating: (0) |
Any ideas guys? Cheers, Matty G |
Follow us on