10/19/2018 11:58 AM | |
Joined: 10/18/2016 Last visit: 3/12/2024 Posts: 21 Rating: (1) |
Hello Marcelo, i guess you are using the CP443-1 Adv (6GK7443-1EX41-0XE0) which does not support the extended PROFINET diagnostics. However the PROFINET IO devices that support the extended PROFINET diagnostics can only be operated on PROFINET IO controllers that likewise support the extended PROFINET diagnostics. Also your devices do not have a migration GSDML file available.. (See also this FAQ: https://support.industry.siemens.com/cs/ww/en/view/23678970) But the successor product of your used CP443-1 Adv (6GK7443-1GX30-0XE0) does support extended PROFINET diagnostics. With best regards, PN-Team |
Follow us on