10/25/2016 8:18 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi graeber, Did you update the SFC block types? See below: 1. Select one or more SFC types in the chart folder of the master data library. 2. Select the menu command Options> Charts > Update Block Types. The "Update Block Types" dialog box opens. 3. Select the S7 programs to be checked for differences compared with the block types/SFC types selected in the master data library. 4. Click "Next". All S7 programs selected are checked and another dialog for selecting the block/SFC types opens. The dialog also provides information about the possible effects of the update of the block/SFC types. 5. Specify the block/SFC types to be updated for the S7 programs. You have selected all block/ SFC types to be updated. You can exclude selected block types from the update, if required. 6. If there are no block/SFC types to be updated, no block/SFC types will be displayed. In this case, close the dialog box. 7. Click "Make". |
If I could help you, you can use the RATE button. Thank you. |
|
10/27/2016 7:48 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi graeber, I was looking into your issue...but saw it was resolved. I don't know why you had to compile the OS twice. That doesn't make sense. |
If I could help you, you can use the RATE button. Thank you. |
|
10/29/2018 1:23 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi Pooran, is the user with the error in the user group "User"? with regards |
Follow us on