11/2/2018 10:01 AM | |
Joined: 10/16/2007 Last visit: 9/11/2024 Posts: 629 Rating: (45) |
Hello, you can use them with S7-1500 too. Regards |
11/2/2018 10:19 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi beisek89, it is not clear what you really need. ET200s can be also used with S7-1500 CPU. I guess you want to change from ET200s to ET200SP. have a look to the ET200SP manual collection. In the part device specific information you will find the manuals of every module of ET200SP-series. I am sure that you find some, that may fit your requirements: SIMATIC ET 200SP Manual Collection hope this helps, regards |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
11/2/2018 1:55 PM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi beisek89, please check the following Link to the following entry: Counting/Position Detection Module TM PosInput 1 for Counting, Measurement and Position Detection in the ET 200SPIt offers a counting channel for difference input signals according to RS422 up to 1 MHz, as well as the position detection with the aid of SSI absolute encoders. For the count functions, the connection of 5 V TTL signals is also possible. Regards, Towome |
|
|
Follow us on