Industry Online Support
Technical Forum
11/5/2018 12:52 PM | |
Joined: 5/18/2018 Last visit: 3/28/2023 Posts: 7 Rating: (0) |
Hi, CPU is in STOP mode The CPU is in Error, and the massage I get in "Diagnostic Status" is : Module exists. faulty Fault LED (SF) Unable to Upload and download any data, At present no memory card in the PLC module, Please tell me, if can we program this PLC without memeory card. AttachmentPROJECT COMMISSION.docx (170 Downloads) |
11/5/2018 1:54 PM | |
Joined: 9/21/2012 Last visit: 9/21/2024 Posts: 4153 Rating: (464) |
You need to have a memory card in the PLC, to be able to use it. |
Follow us on