11/9/2018 6:54 AM | |
Posts: 3 Rating: (0) |
Hi I am trying to make a light automatisation with the LOGO!8 but got some little problems. First of all I have to different kind of armatures, one kind is with 0-10V and the others are with 1-10V. The Left to sections on the program file are 0-10V dimming and this two works fine, I've attached resistors to the analog output of the logo and connect too the armatures. But the one which is combined won't dim. It uses two analog outputs. Another problem is that I need to add an light sensor to automatically dim the lights depending on the outdoor light. I want to do that with only one sensor, is it possible? and how can I get that working, I can't think about how I would do that. Friendly regards, Kenny. AttachmentLOGO!8 automatisation.zip (272 Downloads) |
Last edited by: QuintensK at: 11/9/2018 7:24:06 AM |
|
11/9/2018 7:29 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Thank you. |
11/9/2018 8:21 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
I wrote to the Moderation a suggestion. Then will the moderator move the topic in the right conference. |
11/9/2018 8:27 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Attached is a suggestion how to control two analogue outputs with different voltage values (0-10V and 1-10V) with one dimmer signal. The counter is representative of your dimming function and should give you only the possibility of Simulation. Attachment0-10V_and_1-10V_FS4.zip (300 Downloads) |
Follow us on