11/14/2018 12:19 PM | |
Joined: 10/8/2015 Last visit: 8/26/2024 Posts: 14 Rating: (0) |
Dear all, I had problem with project in TIA Portal V15 as picture.zip file below HMI (TP1500) connect with PLC Device proxy (S7-400 from Step 7 project) via Ethernet (sub net in Step 7 is 00B4-0007, sub net in TIA Portal is 00B4-007 ) PLC Device proxy (S7-400) connect with PLC Device proxy (S7-300 from Step 7 project) via Profibus (sub net in Step 7 is 00B4-000E, sub net in TIA Portal is 00B4-00E ) Now, I make 1 S7 routing connection between HMI (TP1500) and PLC Device proxy (S7-300). But after I download to HMI, the connection cannot get the value from the PLC. Could someone have good idea for this case?
Attachmentpicture.zip (59 Downloads) |
11/16/2018 12:09 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13748 Rating: (1731) |
Hello a S7-routing Connection with 2 Proxies... theoretical It should work if all the components support S7 Routing: https://support.industry.siemens.com/cs/ww/en/view/584459 you can read also the routing ecxample in the Proxy FAQ: https://support.industry.siemens.com/cs/de/en/view/73502293 Bye Murof |
Last edited by: Murof at: 11/16/2018 12:10:08 PMIf this Information really helps, you could use the Rate function |
|
Follow us on