11/20/2018 7:03 AM | |
Posts: 1 Rating: (0) |
Hello Good day I want to set analog input 4-20mA as a reverse . like 4mA will 100 and 20mA will 0 . how to create it on LOGO 0BA6 leder diagram ? If any body know it please let me know. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/20/2018 8:04:32 AMNew subject after splitting |
|
11/20/2018 7:56 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32878 Rating: (4064)
|
In the attachment a simple example. B003 is just a dummy, has no function for the program. B003 is only used to complete blocks B001 and B002. B004 is only for displaying the current in the analog input. Has no function for calculating the output value. AttachmentAnalog_4-20mA=100-0_0BA7.zip (147 Downloads) |
Follow us on