11/22/2018 12:51 PM | |
Joined: 11/15/2017 Last visit: 12/1/2022 Posts: 23 Rating: (0) |
Hello, I am using CPU 1513 and cm ptp card(rs485) over Et200sp. What's happening is communicating was happening one day ago, now the communication has stopped the TX is blinking but the RX is continuously lit up. Also the block is showing status code 7002; data transmission running but there is no data received in Ptr db. Also if checking the slaves loop over modscan I am getting data without any issue. So please help. Also the S_MODE is 0 in my case. Thanks in advance. Regards Raj ------------------------------------------------------------------------------------------ |
Last edited by: rajjamdhade at: 11/22/2018 12:53:17 PMLast edited by: Jen_Moderator at: 11/22/2018 2:20:44 PMNew subject after splitting |
|
11/22/2018 2:37 PM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
Follow us on