7/30/2015 5:18 PM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating: (5) |
Hello I tried to install TIA Portal V13. I could install the following packages successfully: STEP7 PROF V13, STEP 7 PROF SP1 V13.0, and WinCC V13 PROF. However, When I installed WINCC V13 PROF SP1 an error showed up moreover I'm working with a Virtual Machine VMWare with Windows 7 Professional 64 bits SP1. The error is: 12:46:24 | OK RebootAfterAll SetupUnit (SCADA-RT), Complete - - PlusMain, Reinstall 12:46:34 |ERROR SeconWorker::ExecuteSeconWork(): - Secon call has been finished with errors 12:46:34 | FAIL! SecurityControl (SCADA-RT), Failed;After I attached the log file created after the installation.
---------------------------------------------------------------------------------------------------- AttachmentSIA_WINCC_PROFESSIONAL_V13_SP1@15-07-10_11-42-19_summary.txt (621 Downloads) |
Last edited by: Min_Moderator at: 7/31/2015 9:08:19 AMNew subject after splitting |
|
11/29/2018 7:07 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012)
|
Hello, looks like a wrong Windows10 build number. If you have build 1709 or above then the Windows version is not compatible with WinCC V13 SP1. You can try WinCC V13 SP2 or the Secon Fix for Windows 10 1709: https://support.industry.siemens.com/cs/ww/en/view/109755067 Regards Christoph |
Follow us on