Industry Online Support
Technical Forum
1/19/2013 5:58 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, When you use failsafe over Profinet, the modules must comply to Profisafe Profile V2. This is also explained here: http://support.automation.siemens.com/WW/view/en/14196393 This exactly how I understand the error message you got. Can it be that you replaced a Profibus CPU with a PN/DP CPU? And thatsome existing modules in the configurationare older ones (Profisafe V1)? I would also recommend to use a recent configuration pack. Can be found here: http://support.automation.siemens.com/WW/view/en/15208817 |
Best regards |
|
11/30/2018 3:55 PM | |
Joined: 1/17/2018 Last visit: 9/10/2024 Posts: 24 Rating: (2) |
I got the same error, but then I noticed that I didn't have the safe capability of the S7-400H turned on. :) |
Follow us on