11/30/2018 1:19 PM | |
Joined: 4/11/2014 Last visit: 9/13/2021 Posts: 22 Rating: (0) |
Hi everyone. I have a confusion with ET200SP base units. i need to configure 6ES7134-6GF00-0AA1 8ch AI card supports U/I Inputs to a base unit 6ES7193-6BP00-0BA0 without AUX terminals.Is it possible to configure the 4 wire Current input to this base unit 6ES7193-6BP00-0BA0? Because i was referring the drawing of base unit with Aux termials.It doesnt Differ much except the AUX termials are shorted with 0v Supply.. Can anyone tell me what could be the best Base unit? Thanks.. ------------------------------------------------------------------------------------------ |
Last edited by: HarePrasath at: 11/30/2018 1:20:38 PMLast edited by: Jen_Moderator at: 12/3/2018 12:47:35 PMNew subject after splitting |
|
Follow us on