11/29/2018 5:24 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Sandeep Bakoliya, this may be possible, but not with the options of WinCC. The possibilities of Virtualization with WinCC are described in the Application example https://support.industry.siemens.com/cs/ww/en/view/49368181
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
11/29/2018 9:40 AM | |
Joined: 7/20/2015 Last visit: 4/23/2024 Posts: 153 Rating: (27) |
Hi bg2492 Thanks for giving me reply. yes this is right There is only the option "WinCC/Redundancy", where you can But can we configure 4 server in redundancy with one master and rest of all 3 server on stand by? like Physical Server A (Master) Physical Server B (stndby) VM Server A (stndby) VM Server B (stndby) can we do this type of configuration ? Thanks & Regards Sandeep Bakoliya |
Regards |
|
Follow us on