10/31/2018 12:13 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, The Linux environment of the IOT2000 runs independently from Arduino Sketch. So yes, they can run simultaneously, but to exchange data between arduino sketch and python you would have to use MQTT broker or write into a file of the filesystem. If your Arduino sketch is just doing GPRS connection, I would suggest using a 3G mPCIe card instead. Then you can work on the Linux side only, access GPIOs over python, store data in SQL and then push it to a cloud over the 3G mPCIe card. Kind regards! |
This contribution was helpful to1 thankful Users |
12/5/2018 9:22 PM | |
Posts: 13 Rating: (0) |
I took your advice and moved to Linux side. Fortunately, I had an Intel 6205 lying amidst my mess for a few year which I was able to find. So, at least I had Internet access even if that did not come from 3G mPCIe. However, I will be ordering one soon and test it as well with the device. Many thanks for your help! :) |
Follow us on