11/29/2018 9:32 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello matt1115, you should connected the I/O OCCUPIED to, but this isn't the problem. The "BATCH CDV" handles the following three tasks (get more infomation about CDV):
So if the CDV doesn't run no WinCC messages will stored. Sometimes when I start the PC the SQL Sever for CVD wouldn't start automaticly. You can see the status form the sql server and starting and stopping an SQL Server under "Windows menu > all apps > Microsoft SQL Server 20xy > SQL Server 20xy Configuration Manager". |
11/29/2018 1:40 PM | |
Posts: 23 Rating: (2) |
Here is what I see. I tried to start the SQL Server Agent but it did not seem to help remove that error. |
12/6/2018 8:23 PM | |
Posts: 23 Rating: (2) |
I have noticed that my Limit Violations in the Report Say 0. This is not correct. |
Follow us on