12/11/2018 1:39 AM | |
Posts: 2 Rating: (1) |
Hi I am buying a SD card for G120 Sinamics. There are 2 options: Empty card or incl. licensing (Certificate of License) V4.7 SP10 HF1. Part numbers as:6SL3054-4AG00-2AA0and6SL3054-7TF00-2BA0 Can anyone please explain what is the licence for and when it is required? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2018 9:47:07 AMNew subject after splitting |
|
12/11/2018 10:25 AM | |
Joined: 10/11/2006 Last visit: 5/7/2024 Posts: 5834 Rating: (790)
|
Hello, you will get a certificate of license which will come with the SD card with firmware. If you have selected additional licenses, i.e. safety license, you will get an additional certificate of license for the safety license with the shipment. The following passage is out of the V4.7 SP10 HF1 sales and delivery realase (https://support.industry.siemens.com/cs/de/de/view/109755811/en) which describes the available options pretty good. The firmware is included on the SINAMICS G120 multicard, firmware version 4.7 SP10 HF1. |
With best regards, |
|
Follow us on