12/14/2018 8:42 AM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
Hello, unfortunately,, I didnt know about that limitation and I ordered 6ED1052-1MD00-0BA8 Since I ordered it from the net, I am stuck with it because the returning would be too expensive. The question is: what can I do with it regarding to WEB use? Anything at all? At least, I would like to see status of inputs/outputs and program variables over the net or via android phone for a control of process (heat pump for domestic heating)? Can I do that at least? I would like to change the parameters as well (room temperature...) like "teleservice". Can it be done maybe with Siemens Logo application? https://play.google.com/store/apps/details?id=com.siemens.snc.ilogo Or any other way? I think Siemens should sign more clearly that not all 0BA8 are capable of Web use, I am feeling to be mislead and frustrating :( Thank you
------------------------------------------------------------------------------------------ |
Last edited by: Frayer at: 12/14/2018 8:46:27 AMLast edited by: Jen_Moderator at: 12/14/2018 11:33:27 AMNew subject after splitting |
|
12/14/2018 10:01 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32891 Rating: (4066)
|
Yes, it is a standard web page. The sursors keys and F keys of a TDE can you use in this webserver. If you make message texts, you must set the checkmark by Both and Webserver. In attachment a screenvideo. AttachmentWeb server.zip (140 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on