1/25/2018 3:12 PM | |
Joined: 3/17/2014 Last visit: 1/15/2024 Posts: 53 Rating: (12) |
Hi, Attached you'll find a zip file with a step by step guide and the Chrony.tar.gz package that you can install on IOT (tested and working with Example Image v2.1.3) for synchronize your IOT with a NTP Server. Hope you'll enjoy it. AttachmentChrony_installation_EN.zip (554 Downloads) |
This contribution was helpful to5 thankful Users |
2/26/2018 6:13 PM | |
Joined: 7/13/2017 Last visit: 5/16/2023 Posts: 10 Rating: (0) |
Hi Davide, I have as well the Image V2.1.3 on a IoT2040 and need a NTP client. When I saw the article I thought that would be an excellent way to get it without deploying a new image. The installation instructions look straight forward, nevertheless I was not able to get in running yet. Maybe you can help me. During the installation I got error messages abound missing dependencies which should not be a problem because of the force option. (See attachment dependency_error.txt) And the chronyd is running. I changed the chrony.conf to connect to my NTP server, which is a Windows 7 PC running w32tm on standard port 123. (See attachment chrony.conftracking.log). But when I restarted the chronyd I saw in the log file that it tried to access IP 0.0.0.0 and not 192.168.1.8 as configured. (See attachment two). The IP address of the iot2000 is 192.168.1.5. Can you tell me what I did wrong? Thanks and regards, Dietmar AttachmentChrony_installation_problem.zip (353 Downloads) |
Follow us on